Remove Duct

Ducts can be deleted one at a time in the Layout or the List tabs. The delete duct option is included in the right-click menu. To delete a duct, follow the steps below. Ducts that contain conductors can’t be deleted.
  1. Select the duct you want to remove in the Duct Layout Editor. This can be done on either the Layout or the List tabs.
  2. Right-click on the duct and select Delete duct.

    NOTE: If the right-click menu doesn’t display for you right away when viewing the Layout tab, try right clicking on the label in the center of the duct.

    In the List tab only, you can also manually delete the selected duct using the Delete key on your keyboard. This marks the duct with REMOVED and changes the text from black to red.

  3. Click Save to complete the edit in the Duct Layout tab. This does not save the edits to your session. Session edits need to be saved using the Save button in the Session Manager ribbon tab.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.