Named Traces

Optionally, your GIS administrator can create Named Traces. These are pre-configured traces with specific goals or use cases.

TIP: If you are an administrator, see the Configuration Guide topic Tracing Configuration for Named Traces.

Click the Named Trace drop-down to view the trace choices (the image below is just an example, and your Named Traces likely differ).


The Trace Options that have an asterisk do not affect the results of a Named Trace. These options should be natively configured within the trace itself.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.