Layout Editor

Layout Editor tool is found on the ArcFM Editor XI toolbar. Upon clicking the Layout Editor button, the Conduit Manager Layout Editor pane opens.

On this pane, the Select Vault tool is visible toward the upper right. This tool is handy for selecting a vault in your map to view the vault layout on the Select Vault Wall section and the visual details for the ducts on the Duct Layout tab. If you use the ArcGIS Pro Select tool, you won’t see details in the Conduit Manager pane. Therefore, you need to use this for viewing the vault details, and only one vault can be selected at a time.

When a valid conduit feature is selected, its FacilityID is displayed toward the top of the pane. The Duct Layout tab and Duct List tab are displayed under Select Vault Wall when a vault is selected. The Duct List tab displays the attributes for the ducts and their associated features present on the vault wall.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.