Session History Details

Session Manager has a special field on the History tab for notes when a session has been rejected. Audit Note is the last field on the tab when the Rejected step of the session’s workflow is selected.

Session card highlighting the Audit Note on a rejected session

A three-state Session Manager workflow includes the Review assignment as illustrated in the image below. However, a two-state workflow does not have a Review assignment. If a session is rejected in the two-state workflow, the rejection is displayed instead on an Approval assignment.

Session in a three-state workflow displaying the rejected step of its history

When a session is reconciled or posted, those acts are also recorded in the History list. As illustrated in the image below, these are indicated next to an orange bubble labeled Session.

Session History tab showing a reconciled step of the session workflow

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.