Remove Cable

Cables can be deleted from a duct on either the Layout or List tab in Layout Editor. You may remove one cable or multiples with one action.

NOTE: Removing a cable does not change the Available property on the duct but does affect the Occupied property. Removing all cables in a duct sets the Occupied property to false and changes the visual display on the Layout tab.

  1. If you start from the Layout tab, select the duct which contains the cable or cables that you wish to remove.
  2. Right-click and select the Edit cables option.

    The focus shifts to the List tab with the selected cable(s) higlighted.

  3. From the List tab, select one of the remove menu options.
    1. Right click a cable to show the Remove cable option.

    2. Right click on the duct to show the Remove all cables option.

  4. Click Save to complete the edit in Layout Editor. This does not save the edits to your session. Session edits need to be saved using the Save button in the Session Manager ribbon tab.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.