Correction Assistant

The Correction Assistant offers a workflow within the ArcFM Validation Assistant to automatically apply the rule of choice to repair the validation error.

The Correction Assistant gives the option to fix the selected pair (also referred to as an Item) or an entire group, if the group breaks the same rule.

The Correction Assistant can also apply Asset Types to both ends of the validation error. However, it only applies fixes to Junction-Edge or Junction-Junction type rule validations.

When a rule is successfully applied, the Validation Assistant displays a confirmation message to the user and offers guidance on the next steps. The validation error repaired with the correction is also removed from the list of validation errors.

While applying the change, if an error occurs (e.g., from the violation of an attribute rule) a red error message is displayed. Research into attribute rules should be done before informing Schneider Electric Support.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.