Delete Component Tool

The Delete Component tool on the Component Information pane deletes the selected feature and all it’s contained features, and it also removes any associations it may have.

Upon clicking the Delete Component button, a dialog displays informing it will delete all contained features and asking if you want to continue. Click Yes to continue.

After a moment, a dialog displays indicating the feature and its contained features have successfully deleted.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.