Targets

The Targets pane allows users to create a targeted list of Esri Templates for use when completing work. Users can edit Target attributes before placing the feature on the map, thus quickly creating features with the desired attributes. Targets are saved in the local project file, which means they are saved within a map project and are included in published map projects. This is one way to share Targets with others, you can also share a copy of your local project file to share targets you have created.

Click the Targets button to open the Targets pane. If there are any Targets already present in the map, they display on this pane. Otherwise, the display states no targets exist yet.

To create Targets, see Send to Targets for more info.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.