ArcFM Assign Phase

The ArcFM Assign Phase tool was built to automatically apply the phase designation of the snapped origin feature to any newly sketched features. The tool also supplies you with the ability to include choosing the phases you want present without having to adjust them in an attributes table. This tool reduces the number of clicks and context switches regarding placing new service drops or even creating a new feeder. The ArcFM Assign Phase tool can also be applied to group templates.

  1. Select a feature template to sketch.
  2. Click the ArcFM Assign Phase button.
  3. Start your sketching workflow.
  4. An interactive dialogue displays when sketching is complete.
  5. If the sketch has no origin feature, all 3 phases are selected by default. If there is an origin feature, the template selects the same phases that the origin feature has configured.
  6. After the phases are selected, click OK to apply the phases to the newly sketched feature. The phases specified in the template are applied to the Phases Normal attribute in the feature.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.