Remove Duct Bank

An entire duct bank is removed with a few steps, as outlined below. Only duct banks with unoccupied ducts can be deleted.
  1. On the List tab of the Layout Editor, right-click on the duct bank you want to delete.
  2. Click Delete entire duct bank.

    The duct bank is then marked as MODIFIED and all the ducts contained within the duct bank are marked as REMOVED.

  3. Click Save to apply the edit. This may take a moment to complete.
    TIP: The save button only applies your edits, it does not save the edits in your session.

    If you try to delete a duct bank with currently occupied ducts, the Delete entire duct bank option is disabled and a pop-up displays indicating a duct bank with occupied ducts can’t be deleted.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.