Downstream and Upstream Protective Device Traces

Applying the Protective Network Category to the desired ASSETTYPES results in their participation in protective device traces. Similar to Downstream and Upstream traces, the Downstream Protective Device Trace will produce the trace results of Protective features downstream of the starting point while the Upstream Protective Device Trace will produce the trace results of Protective features upstream of the starting point all the way up to the source.

For additional information, see the Network Categories for Tracing topic.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.