View Associations Mode

Users can choose to view associations or turn them off on the Component Information pane using the Turn View Associations Mode On/Off tool. When the tool is turned on, the background of the button it turns green .

When the tool is turned off, no associations are visible on the map:

When the tool is turned on, the associations are visible as dashed lines:

TIP: This tool is also found on the Utility Network Data ribbon with the same icon and is labeled with View.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.