View Gas Devices

Gas & Water:

You are presented with an open and close user interface drawing of a ball-valve that is governed by the Device Status field.

  1. Select a controllable feature then click the Component Info tool. Alternatively, you can click Component Info then select the controllable feature.

  2. Toggle the phases or valve setting by clicking on the UI element.

    TIP: For best results, click within the circle on phases and on the colored part of the valve.
  3. You are presented with a dirty area that must be validated before any Geoprocessing (e.g., tracing) can be performed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.