Downstream and Upstream Traces

Downstream traces produce trace results for features that are downstream from the starting point of the trace as long as those selected features are not blocked by the condition barrier designated by the subnetwork’s tier configuration. These features must also match either the selected phase per the trace wheel in the multi-phase scenario or the phase of the starting feature when in the single-phase scenario.

Upstream traces produce trace results for features that are upstream of the starting point on the way to the source of the subnetwork (subnetwork controller). This trace also adheres to the same rules the downstream trace follows.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.