Edit Vaults

Vaults are an important component of a successful conduit network and are required to take advantage of Editor XI Conduit Manager functionality. Vault features are created using out-of-the-box Esri editing tools.

The Vault Orientation in the Layout Editor pane doesn't respond directly to edits made in ArcGIS Pro. This means geometry edits to a vault wall while the vault is selected in the Layout Editor, do not display automatically. For the new edits to display, you must re-select the vault again with the Select Vault tool.

It's important to ensure the vault polygon is correct and final before adding duct banks and ducts to the vault's walls. It is very difficult to restore the geometric coincidence of existing ducts with the vault outline after modifying the shape of the vault outline in any way.

IMPORTANT: Before using the Create Duct Bank tool to create a duct bank between two vault features, make sure the WallHeight attribute for each of the vaults is populated. It must be populated in the same units as your map, for example, in feet if your map units are in feet, or in meters if your map units are in meters. The Z value for vaults is measured at the ceiling of the vault polygon (not the floor). For example, a vault with a Z value of 0 (ceiling is at ground level) and a wall height of 3, means your duct bank Z value must be between 0 and -3.

View Vaults in 3D

A Vault feature is modeled in GIS as a planar polygon, which the ArcFM Conduit Manager data model interprets as representing the ceiling of the vault. Since the Vault feature also gives the height of its walls via the WallHeight attribute, it is possible to display the vault as a 3D figure with volume in an ArcGIS Pro 3D Scene by extruding the ceiling (i.e. the polygon) downward by the amount given in the WallHeight attribute. This allows you to visualize not just the ceiling of the vault, but also the walls and the floor, and to see the positions of the DuctEnd features on the walls. Follow the steps below to set up Extrusion for vault features in a 3D Scene to achieve this effect.
  1. Add Structure Boundary to a Scene in ArcGIS Pro. For more information on how to use Scenes, read more at the Esri Scenes topic.

  2. Select the Structure Boundary feature layer in the Scene’s Contents pane.

  3. Click the Feature Layer tab.

  4. Expand the Type drop-down and select either Min Height or Max Height from the list (either works the same).

    Type drop-down field options on the Feature Layer tab

  5. Select Wall Height from the Field drop-down. This setting allows values entered in the WallHeight field to be displayed in a 3D form on the map.

  6. Ensure that the Unit value matches the unit of measure used in your map.

  7. Click the Extrusion Expression Expression button.

  8. The Expression Builder dialog opens. In the Expression field, add a – (minus) sign in front of the existing expression so the expression now reads:

    -$feature.wallheight

    Expression Builder dialog

  9. Click OK. The Field value changes from WallHeight to Custom.

This is an example of how the vault looks before and after extrusion is set up.

Vault Before Extrusion

Vault After Extrusion

Vault before extrusion

Vault after extrusion

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.