Duct Bank Availability

There are several ways to tell if a duct is available or occupied in the Conduit Manager Layout Editor Pane. This is helpful to discern whether a duct has room for additional cables at a quick glance.

In the List tab of the Conduit Manager Layout Editor pane, at the top of the list Duct bank indicates how many ducts are still available.

On the Duct Layout tab, an available duct is filled in white, an occupied duct is filled in grey. A darker shade of grey indicates the duct is at capacity and can't fit any more cables, where a lighter grey indicates the duct is occupied but still has room for additional cables within it.

Duct Attributes in the Conduit Manager Layout Editor allow you to check if a duct is available or occupied. When Available is checked, it indicates there is room for cables in the duct. If Occupied is checked, it indicates there is at least one cable present in the duct.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.