Operate Electric Devices

Click each phase to operate individually. Further, Component Information offers a way to operate all switches at once if the contained switch assembly envelopes three switch devices with the applied Disconnect network category.

IMPORTANT:

The Disconnect Network category must be applied to any AssetType in the Electric data model so an editor can use Component Info to operate the feature.


The Open or Close All Phases buttons are enabled based on the state of the contained devices upon selection of the assembly.

  • If all the contained switches are closed, the Open All Phases button is enabled.

  • If all the contained switches are open, the Close All Phases button is enabled.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.