Multi-Phase Tracing

When you use any electric trace tool on any feeder with more than one phase, you are presented with the phase trace wheel shown below. Selecting any of the options on the wheel produces results that have any combination of the designated phase (e.g. a trace on A phase will select any features that have ABC, AC, AB, or A in their PhasesNormal field).

When the starting location is a feature of a SINGLE PHASE, the trace wheel is not presented and the trace selects results based on the condition of that single phase.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.