View Component Information

There are several ways to view a component in Component Information.

  • Load Selected from the Component Information pane:

    • After launching Component Info, select a feature in the map, then click the Load Selected button to display the component information for that feature.

  • Using the map:

    • Right-click on a feature in the map, then click the Component Info button.

  • Using the Attribute Viewer pane:

    • Right-click on a feature in Attribute Viewer, then click the Component Info button.

  • Using the ArcFM Search Results pane:

    • Click the Component Info button next to a feature to view its details.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.