Delete a Session

The steps below walk you through deleting sessions in Session Manager.
  1. From any of the Work tabs, (My Work, Available Work, or Assigned Work) select a session in the left side of the Session Manager dialog.
  2. Click the Delete button. A confirmation message appears confirming your request to delete.
    Message confirming the user wants to delete the selected session
  3. Click Yes to continue deleting the selected session. A confirmation message appears confirming the session was deleted. It’s important to note that when a session is deleted, the associated version is also deleted.
    Message confirming all selected sessions have been deleted
To delete multiple sessions, use the Shift or Control key to build your selected set of sessions. The session card displays the number of sessions selected. Click Delete All Selected Sessions.

Session Manager dialog with multiple sessions selected and Delete button highlighted

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.