Open a Session on an Existing Version

When a project is opened, Editor XI checks if you have a previously saved session linked to the project (or map version). If so, you are prompted if you want to open the associated session.

Message with option to open session associated with a map version

Click Yes to open the associated session or click No to switch to Default.

If no associated session is found for the user, the Matching Session Not Found message displays.

Message indicating that no session was found associated with the current map version

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.