DOCA0157EN-09

Commissioning

  • The PowerTag Link gateway uses an internal self-signed certificate by default.

  • During the commissioning phase, user intervention is not required when dealing with product certificate management.

  • User can configure the device to use the product certificate which is provided by the end-user.

  • User can delete a certificate which he uploads and he cannot delete a self certificate.

Certificate regeneration is automatic, and is activated in two cases:

  • When the certificate has expired or when imported certificate has been deleted.

  • During the deletion of the imported certificate.

The features of Imported Certificate Obligatory are:
  • File: PCKS12 (see following Note)

  • Encryption: RSA≥2048 bit or ECC≥256 bit

  • Signature: RSA256

  • Key Usages: Digital Signature and Key Encryption

  • Extended Key Usages: Server Authentication

  • Format: X509 v3

NOTE: For firmware versions lower than 002.002.002, .pfx or .p12 format is supported. For firmware versions 002.002.002 and above, only the .pem format is supported when importing a user-signed certificate. If you have the .pfx format, convert it to .pem (for example by using a tool such as OpenSSL) before importing it.

If a user-signed certificate has already been imported into the previous firmware version, it is automatically deleted when the firmware is updated and a self-signed certificate is generated. You are informed via a pop-up message.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.