DOCA0157EN-09

Modbus Table Format and Data Types

Table Formats

Register tables have the following columns:

Address

Register

No.

RW

X

Unit

Type

Range

Default Value

Svd

Function Code

Applicable Devices

Description

Designation

Description

Address

16-bit register address in hexadecimal. The address is the data used in the Modbus frame.

Register

16-bit register number in decimal. Register = Address + 1

No

Number of 16-bit registers that need to be read/written to access the complete information

R/RW

Whether the register is read only (R/RW) or read-write (RW).

X

Scale factor:

  • A scale of 1 means that the value of the register is the right one with the unit indicated.

  • A scale of 10 means that the register contains the value multiplied by 10. The actual value is therefore the value of the register divided by 10.

  • A scale of 0.1 means that the register contains the value multiplied by 0.1. The actual value is therefore the value of the register multiplied by 10.

Unit

Information unit of measurement:

  • ”: no unit corresponding to the value expressed.

  • “h”: hours

  • “D”: the unit depends on the connected device.

Type

Coding data type (see Data type table below).

Range

Range of permitted values for the variable, usually a subset of what the format allows. For BITMAP type data, the content of this domain is “–”.

Default Value

Default value for the variable

Svd

Value saved when the power supply to the PowerTag Link gateway is switched off:

  • “Y”: the value of the register is saved.

  • “N”: the value is lost.

NOTE: On start-up or reset, the available values are retrieved.

Function code

Code of functions that can be used in the register.

Applicable Devices

Code indicating the types of devices for which the register is available.

Description

Information about the register and the restrictions that apply.

Data Types

Name

Description

Range

INT16

16-bit signed integer (1 word)

-32768...+32767

UINT16

16-bit unsigned integer (1 word)

0...65535

INT32

32-bit signed integer (2 words)

-2 147 483 648...+2 147 483 647

UINT32

32-bit unsigned integer (2 words)

0...4 294 967 295

INT64

64-bit signed integer (4 words)

-9 223 372 036 854 775 808...9 223 372 036 854 775 807

UINT64

64-bit unsigned integer (4 words)

0 to 18 446 744 073 709 600 000

Float32

32-bit value (2 words)

-3.4028E+38... +3.4028E+38

ASCII

8-bit alphanumeric character

Table of ASCII Characters

BITMAP

16-bit field (1 word)

DATETIME

Refer to DATETIME

NOTE:

Float32 type data: Single precision float with sign bit, 8 bits exponent, 23 bits mantissa (positive and negative normalized real)

For ASCII type data, the order of transmission of characters in words (16-bit registers) is as follows:

  • Character n as least significant

  • Character n + 1 as most significant

All registers (16-bit or 2 bytes) are transmitted with Big Endian coding:

  • The most significant byte is transmitted first.

  • The least significant byte is transmitted second.

32-bit variables saved on two 16-bit words (e.g. consumption meters) are in Big Endian format:

  • The most significant word is transmitted first, then the least significant.

64-bit variables saved on four 16-bit words (e.g. dates) are in Big Endian format:

  • The most significant word is transmitted first, and so on.

DATETIME

DATETIME is a data type used to code date and time defined by the IEC 60870-5 standard.

Register

Type

Bit

Range

Description

1

INT16U

0–6

0x00–0x7F

Year:

0x00 (00) to 0x7F (127) correspond to years 2000 to 2127

For example, 0x0D (13) corresponds to year 2013.

7–15

Reserved

2

INT16U

0–4

0x01–0x1F

Day

5–7

Reserved

8–11

0x00–0x0C

Month

12–15

Reserved

3

INT16U

0–5

0x00–0x3B

Minutes

6–7

Reserved

8–12

0x00–0x17

Hours

13–15

Reserved

4

INT16U

0–15

0x0000–0xEA5F

Milliseconds

Direct Bit Addressing

Addressing is permitted for BITMAP type zones with functions 1, 2, 5, and 15.

The address of the first bit is constructed as follows: (register address x 16) + bit number.

This addressing mode is specific to Schneider Electric.

Example: For functions 1, 2, 5, and 15, bit 3 of register 0x0078 should be addressed; the bit address is therefore 0x0783.

NOTE: The register whose bit needs to be addressed should have an address ≤ 0x0FFF.

Example of Modbus Frames

Request

Definition

Number of Bytes

Value

Comment

Server number

1 byte

0x05

PowerTag Link Modbus Address

Function code

1 byte

0x03

Reads n output or internal words

Address

2 bytes

0x36E2

Address of a consumption meter whose address is 14050 in decimal notation.

Number of words

2 bytes

0x002C

Reads 44 16-bit registers.

CRC

2 bytes

xxxx

Value of CRC16.

Response

Definition

Number of Bytes

Value

Comment

Server number

1 byte

0x05

PowerTag Link Modbus Address

Function code

1 byte

0x03

Reads n output or internal words

Number of Bytes

2 bytes

0x0058

Number of bytes read

Value of words read

88 bytes

Reads 44 16-bit registers

CRC

2 bytes

xxxx

Value of CRC16.

Modbus Register

The address of register number n is n-1. The tables detailed in the following parts of this document provides both register numbers (in decimal format) and corresponding addresses (in hexadecimal format). For example, the address of register number 3000 is 0x0BB7 (2999).

NOTE: To know the description of the registers of each associated device (how to use them), print the PDF report of Modbus registers using EcoStruxure Power Commission software (refer to EcoStruxure Power Commission Online Help). This report gives a dynamic knowledge of all the registers potentially to be integrated into the supervision systems including a description of each register.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.