DOCA0157EN-09

Communication Diagnostics

Ethernet

Step

Action

1

Launch the PowerTag Link webpage in the web browser.

2

Login with user name and password.

3

Click Diagnostics > Communication > Ethernet.

The Ethernet page displays the global and port statistics of the Ethernet network.

 

Function Name

Description

Ethernet Global Statistics

Frames Received OK

Displays the number of frames received from all the Ethernet ports.

Frames Transmitted OK

Displays the number of frames transmitted from all the Ethernet ports.

Reception Errors

Displays the number of errors during reception of the frames.

Ethernet Port Statistics

Link speed

Displays link speed on Ethernet port.

Duplex mode

Displays the communication mode of the Ethernet port. It can be half duplex or full duplex.

Click Reset to clear the Ethernet frame counters.

IP Network Services

Step

Action

1

Launch the PowerTag Link webpage in the web browser.

2

Login with user name and password.

3

Click Diagnostics > Communication > IP Network Services.

 

Function Name

Description

Modbus TCP Port

Port status

Displays the current status of the Modbus/TCP port.

Opened TCP connections

Displays the number of established Modbus/TCP connections.

Received messages

Displays the counter of received Modbus/TCP messages.

Transmitted messages

Displays the counter of transmitted Modbus/TCP messages.

Modbus TCP Port Connections

Displays the statistics of open Modbus/TCP connections.

Click Reset to clear the Modbus/TCP counter.

Wireless Network Quality Indicators

Step

Action

1

Launch the PowerTag Link webpage in the web browser.

2

Login with user name and password.

3

Click Diagnostics > Communication > Wireless Network Quality Indicators.

The Wireless Network Quality Indicators page displays wireless network quality information such as Link Quality Indicator (LQI), Received Signal Strength Indicator (RSSI), and Packet Error Rate (PER).

Parameter

Description

Modbus Address

Displays the Modbus address of the wireless device.

Asset Name

Displays the user-defined asset name of the wireless device.

Usage

Displays the user-defined usage of the wireless device.

Product

Displays the type of wireless sensor.

LQI

Displays the measurement of the strength and / or quality of the received frames.

The following values of LQI indicates the quality of the received frames:

  • The value from 0...29 indicates that the RF communication is bad. In this case, check whether the rules of installation are followed. You can also change the location of the PowerTag Link gateway inside the panel to be near to the wireless device.

  • The values from 29...59 indicates that the RF communication is average. In this case, look at the RSSI value whether to accept the level of quality or not. If the RSSI is above limit, consider the value of LQI as acceptable.

  • The value greater than 59 indicates that the RF communication is OK.

NOTE: It is recommended to use this indicator as the main indicator of acceptance.

Radio Quality

Displays the quality of the frames. When the LQI value is greater then 59, it indicates with green light and when LQI value is lesser than 29, it indicates with red light. When the LQI value is between 30 and 59, it indicates with orange light.

RSSI

Displays the power level of the wireless signal between the PowerTag Link gateway and the wireless device.

  • Good: 0...-65 dbm

  • Average: -65...-75 dbm

  • Bad (with risk of outage): < -75 dbm

PER

Displays the ratio of the packet that does not reach a destination over the total expected number of packets and is expressed in percentage. For PowerTag Link gateway, the ratio is calculated over a fixed window of five minutes.

Email Service

Step

Action

1

Launch the PowerTag Link webpage in the web browser.

2

Login with user name and password.

3

Click Diagnostics > Communication > Email Service.

The Email Service page displays the information such as number of emails sent and emails not sent. This page also displays the error count, if any, for connection errors, authentication errors, internal errors, and sending errors as shown in the following figure:

Parameter

Description

Email Sent successfully

Displays the total number of successfully sent emails.

Emails Not Sent

Displays the total number of emails not delivered to the recipients.

Connection Errors

Displays the total number of connection errors if a connection is lost during an email delivery.

Authentication Errors

Displays the total number of authentication errors.

Internal Errors

Displays the total number of internal errors during the email service.

Sending Errors

Displays the total number of sending errors.

Click Reset to clear the Email counter.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.