DOCA0157EN-09

General Diagnostics

Date/Time

Step

Action

1

Launch the PowerTag Link webpage in the web browser.

2

Login with user name and password.

3

Click Diagnostics > General > Date/Time.

The Date/Time page displays the following information:

Parameters

Description

Date/Time

Date

Displays the current date in the format YYYY-MM-DD.

Time

Displays the current in the local time zone in the format hh:mm:ss.

Uptime

Displays the elapsed time since the last restart of the device.

Last Date/Time Synchronization

Last Synchronization

Displays when the last synchronization happened.

Last Synchronization Time Source

Displays the time source of the last synchronization.

Last Synchronized Date

Displays the last synchronized date in the format YYYY-MM-DD.

Last Synchronized Time

Displays the last synchronized time in the format hh:mm:ss.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.