DOCA0157EN-09

Unpairing Disconnected Wireless Devices

Step

Action

1

Navigate to Settings > Devices > Wireless Devices to view the list of the paired wireless devices.

2

Click the bin icon of the required wireless device to unpair.

Result: A message appears on the screen to confirm the removal of the wireless device from the configuration.

3

Click Yes.

If the device is disconnected or turned off, an error Delete Failed is displayed on the screen.

After few seconds, the below error message is displayed on the screen:

NOTE: If the wireless device is still paired to the PowerTag Link gateway, use the local unpairing method to force the wireless device to unpair. Refer the instruction sheet of the specific wireless device for the local unpairing procedure.

4

Click Yes to initiate the deletion process.

Result: Once the wireless device is successfully deleted, it will not be visible in the list of wireless devices discovered.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.