DOCA0157EN-09

Ethernet Settings

The Ethernet page is used to configure the frame format and speed and mode of the Ethernet port. This page also displays the MAC address of the Ethernet network.

Step

Action

1

Launch the PowerTag Link webpage in the web browser.

2

Login with user name and password.

3

Click Settings > Communication > Ethernet.

Follow the procedure to configure the Ethernet parameters:

Step

Action

1

Select the type of Ethernet frame format from the Frame Format list. It can be Ethernet II, 802.3, or Auto. The default value of the frame format is Auto.

2

Select the value for speed and mode of the Ethernet port from the Speed and Mode list.

The value of speed and mode can be one of the following:

  • 10 Mbps - Half duplex

  • 10 Mbps - Full duplex

  • 100 Mbps - Half duplex

  • 100 Mbps - Full duplex

  • Auto-negotiation

The default value is Auto-negotiation.

3

Click Apply Changes and then click Reboot to automatically restart the device to save the settings. Click Cancel Changes to revert the settings.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.