DOCA0157EN-09

Total Active Power

This alarm indicates that the Total Active Power is greater or lower than the configured threshold value. The alarm will become inactive if the Total Active Power remains under or over (as defined by the comparator) 90% of the threshold value.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.