DOCA0157EN-09

Load Operating Time Counter

This alarm indicates that the load operating time counter has reached the configured threshold value. The time is only taken into account when the current has been above the threshold value for one minute. The alarm can be set with the following conditions:

  • Greater than: The alarm is triggered when the Load Operating Time Counter value exceed the configured threshold value.

  • Every: The alarm is triggered every time the Load Operating Time Counter value has reached the time configured in the threshold value.

    When an alarm is triggered, the system manager receives the email notification and he commissions the loop of the alarm.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.