DOCA0157EN-09

Load Monitoring

Description

The Monitoring page is used to monitor the electrical loads. The facility managers can check the health of the electrical loads such as HVAC, lighting, pumps, and machines.

General Page

The General page displays the status of the load.

Step

Action

1

Launch the PowerTag Link webpage in the web browser.

2

Login with user name and password.

3

Click Monitoring > General.

The following information is displayed for the load:

Parameter

Description

Asset Name

Displays the name of the equipment or load name that the PowerTag Link gateway tracks.

Usage

Displays the usage of the energy of the equipment or load (for example, cooling, lighting, and IT loads.)

Product

Displays the type of PowerTag Link gateway associated to a circuit breaker.

Gateway

Displays the gateway connected to the PowerTag Link gateway.

Partial Energy

Displays the partial counter of energy for the given electrical asset.

Load by Phase

Displays the percentage of the load of the feeder connected to the PowerTag Link gateway. The percentage indicates how far an user is away from the tripping of a circuit breaker. It is the ratio of the actual current to breaker rating.

Green: Indicates the circuit is loaded up to 50% in regards to circuit breaker rating.

Orange: Indicates the circuit is loaded between 50% and 80%.

Red: Indicates the circuit is loaded above 80% versus circuit breaker rating.

Click the expand button to see the real-time data for each device.

For example, the following screenshot shows all the real-time data available for each wireless device:

NOTE: The voltage and current measurements displayed in the PowerTag Link webpages are the RMS values.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.