DOCA0157EN-09

Login into Webpages

Login Page

The Login page is used to enter the user credentials and select the preferred language to access the PowerTag Link webpages. When the user connects to the PowerTag Link gateway through a web browser, the Login page is displayed as shown in the following figure:

Enter the following details in the Login page:

  • Language

  • User name

  • Password

WARNING
POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY, AND CONFIDENTIALITY
Change default passwords at first use to prevent unauthorized access to device settings, controls, and information.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Enter the user name and password to access the webpages related to PowerTag Link gateway. The default user name and password is admin to access the webpage for the first time. You can select the language in the Login page so that all the pages are displayed in the selected language.

The top right corner of all the webpages displays the following information:

  • User name

  • Logout

The Logout link is used to logout of the PowerTag Link webpage.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.