DOCA0157EN-09

Synthesis Table Identification

Identification and Status Register

Address

Register

No.

RW

X

Unit

Type

Range

Invalid Value

Svd

Function Code

Applicable Devices

Description

0x0001

2

1

R

NA

NA

UINT16

NA

9120

Y

 03,

100–4

Product ID of the synthesis table

0x0002

3

16

R

NA

NA

ASCII

NA

0x00

Y

 03,

100–4

Manufacturer name: Schneider Electric

0x0012

19

16

R

NA

NA

ASCII

NA

0x00

Y

 03,

100–4

Commercial reference of the gateway

0x0022

35

8

R

NA

NA

ASCII

NA

0x00

Y

 03,

100–4

Product range of the gateway

0x002A

43

8

R

NA

NA

ASCII

NA

0x00

Y

 03,

100–4

Product model

0x0032

51

10

R

NA

NA

ASCII

NA

0x00

Y

 03,

100–4

Asset name

0x003C

61

17

R

NA

NA

ASCII

NA

0x00

Y

 03,

100–4

Vendor URL string default value: https://www.se.com

0x004D

78

1

Reserved

Gateway Data

Address

Register

No

RW

X

Unit

Type

Range

Invalid value

Svd

Function Code

Applicable Devices

Description

0x004E

79

1

R

NA

NA

UINT16

NA

0xFFFF

Y

 03,

100–4

Gateway product identifier

0x004F

80

16

R

NA

NA

ASCII

NA

0x00

Y

 03,

100–4

Gateway product code / commercial reference

0x005F

96

6

R

NA

NA

ASCII

NA

0x00

Y

 03,

100–4

Gateway firmware version

0x0065

102

10

R

NA

NA

ASCII

NA

0x00

Y

 03,

100–4

Gateway serial number

0x006F

112

8

R

NA

NA

ASCII

NA

0x00

Y

 03,

100–4

Gateway product model

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.