DOCA0157EN-09

Digital Input Switch

This alarm is applicable only for PowerTag control 2DI module. It is triggered when the circuit breaker being monitored is in open or tripped position.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.