DOCA0157EN-09

Function 43-16: Write Date and Time

Structure of Modbus Write Date and Time Messages

Request

Definition

Number of Bytes

Value

Example

Server number

1 byte

0x2F

47

Function code

1 byte

0x2B

43

Sub-function code

1 byte

0x10

16

Reserved

1 byte

0x00

Reserved

Date and time(1)

byte 1

not used

1 byte

0x00

Not used

byte 2

Year

1 byte

0x0A

Year 2010

byte 3

Month

1 byte

0x0B

Month of November

byte 4

Day of the month

1 byte

0x02

Second day of the month

byte 5

Hour

1 byte

0x0E

14 hours

byte 6

Minute

1 byte

0x20

32 minutes

byte 7 and byte 8

Millisecond

2 bytes

0x0DAC

3.5 seconds

(1) Refer to DATETIME.

Response

Definition

Number of Bytes

Value

Example

Server number

1 byte

0x2F

47

Function code

1 byte

0x2B

43

Sub-function code

1 byte

0x10

15

Reserved

1 byte

0x00

Reserved

Date and time(1)

byte 1

Not used

1 byte

0x00

Not used

byte 2

Year

1 byte

0x0A

Year 2010

byte 3

Month

1 byte

0x0B

Month of November

byte 4

Day of the month

1 byte

0x02

Second day of the month

byte 5

Hour

1 byte

0x0E

14 hours

byte 6

Minute

1 byte

0x20

32 minutes

byte 7 and byte 8

Millisecond

2 bytes

0x0DAE

3.502 seconds

(1) Refer to DATETIME.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.