DOCA0157EN-09

Security Recommendations for PowerTag Link Gateway Decommissioning

The product is configured with the sensible information, which includes user account identifiers and passwords, and cryptographic keys.

When disposing the product, it is required to perform a reset level 2 of the product (Refer to Reset Button) to make sure that no sensible or confidential information can be disclosed or reused.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.