DOCA0157EN-09

Selective Pairing of Wireless Devices with Webpages

Step

Action

1

Open a text editor program and create a .csv file containing the RF-id of the wireless devices that you want to pair with the gateway. The Modbus addresses will be assigned to the wireless devices according to the order of their RF-id in the file.

For example, as shown in the following screenshot:

  • Modbus address 1 will be assigned to the wireless device with RF-id = E2079424

  • Modbus address 2 will be assigned to the wireless device with RF-id = E2079439, and so on

2

Login to the webpage. Refer to Login into Webpages.

3

Navigate to Settings > Communication > Wireless Network Configuration.

4

If specified in the radio frequency plan, choose the right communication channel in the Communication tab.

5

Navigate to Settings > Devices > Wireless Devices > Selective Wireless Device Scanning.

6

Click Import to import the .csv file.

Result: A confirmation message is displayed.

7

Scan the environment to discover the imported list of wireless devices.

For more information on discovering the wireless devices, refer to Pairing Principle.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.