DOCA0157EN-09

Current I

This alarm indicates that the Current I is greater or lower than the configured threshold value. The alarm will become inactive if the Current I remains under or over (as defined by the comparator) 90% of the threshold value.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.