DOCA0157EN-09

Configuration Procedure of PowerTag Energy ●63 and M250/630 with Webpage

Step

Action

1

Navigate to Settings > Devices > Wireless Devices to view the list of the paired wireless devices. For more information on discovering the wireless devices, refer to Pairing Principle.

Result: A list of paired devices is displayed.

2

Select any wireless device and click the pencil icon to modify the configuration of the selected energy monitoring device.

Result: The parameters of the energy monitoring devices are displayed.

NOTE: The PowerTag Energy F160 and Rope have additional parameters. Refer to Configuration Procedure of PowerTag Energy F160 and Rope with Webpage.

3

Enter the Asset Name of the wireless device.

4

Enter the Label of the wireless device.

5

Select the Usage.

6

Select the Phase Sequence to define the phase sequence of the meter depending on the way the physical panel is wired (from left to right).

7

Select the Mounting Position.

  • Top: The PowerTag sensor is mounted on the top of the device (circuit breaker or switch-disconnector).

  • Bottom: The PowerTag sensor is mounted at the bottom of the device (circuit breaker or switch-disconnector).

8

Select the Power Supply position.

  • Top: The power supply is connected on the top power terminals of the device (circuit breaker or switch-disconnector).

  • Bottom: The power supply is connected on the bottom power terminals of the device (circuit breaker or switch-disconnector).

9

Select the breaker rating from the Associate Breaker Rating (A) list to calculate the percentage of loads.

10

If requested, enter the value for the energy counter in the Partial Energy area. Click Reset or enter the value as 0 to reset the partial energy counter.

11

Load Operating Time Counter (hours): The Load Operating Time counter indicates the running operating time of the load in hours. The load is powered and power flows to/from the load above the set threshold value. The default value in this field is 60 seconds. You can set this value between 60 seconds and 1000000 hours.

12

Load work when Power is >=: The Load Operating Time counter increments only when the power is greater or equal to the value set. You can set the value between 10 W and 15000 W.

13

Click Apply Changes to save the settings. Click Cancel Changes to revert the settings.

NOTE: It is recommended to create a backup file saved on your PC using the backup function available in the Maintenance menu of the webpage. The file will be automatically saved under the name backup.dat. It will be used in case of dysfunction and replacement of the gateway.

For more information, refer to Inoperative Gateway Replacement.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.