DOCA0157EN-09

Webpages Layout

Description

The webpages can be used for two main operations:

  • Monitoring page allows to check the health of the electrical devices such as HVAC, lighting, pumps, and machines.

  • Gateway settings allows

    • setting of Ethernet parameters and wireless devices parameters.

    • diagnosis of exchanges on Ethernet network.

    • adding or removing wireless devices connected to the gateway.

    • management of time setting and time zone selection.

    • IP configuration and IP services

    • IP filtering

    • configuration of email accounts

    • management of user accounts

    • alarm configuration

Webpages are accessible to the following three categories of user:

  • Administrator can access all information and modify the parameters in the Settings menu.

  • Operator can access monitoring pages of the connected devices and get access to Diagnostic menu.

  • Guest can access only Monitoring menu.

The scope of products supported in the webpages are:

  • PowerTag Link gateway

  • Wireless devices

Webpage Organization

A

Displays the measurements and alarms associated to the devices.

B

Communication diagnostics

C

Performs the backup and restore operation

D

Wireless network configuration

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.