DOCA0157EN-09

Function 8: Modbus Diagnostics

Structure of Modbus Messages Concerning PowerTag Link Gateway Diagnostic Counter Management

Request

Definition

Number of Bytes

Value

Server number

1 byte

0xFF

Function code

2 bytes

08 (0x08)

Sub-function code

2 bytes

22 (0x0016)

Operation code

2 bytes

1 ((0x0001) see below list for operation code)

Diagnostic control

2 bytes

0x0100 (see below list for diagnostic control)

Starting entry index

1 byte

0x00 (0 to 255)

The operation code field is used to select the diagnostic and the statistic data to be read from the device.

Most Significant Byte

Least Significant Byte

15

14

13

12

11

10

9

8

7

6

5

4

3

2

1

0

Reserved

Protocol Version

Operation Code

Bit assignments are included in the table below:

Bit

Field

Description

15...12

Reserved

Must be zero

11...8

Protocol Version (PV)

Indicates version of the protocol of the client (requestor)

Values are: 0x00 (initial version)

7...0

Operation Code

Indicates function to be performed by the command

Values are:

  • 0x01 = Read diagnostic data

  • 0x02 = Clear diagnostic data

  • 0x03 = Clear all diagnostic data

  • 0x04 = List ports

The diagnostic control field provides the data selection information for this protocol as well as specifies the logical port from which, the data is to be retrieved (if applicable). The diagnostic control field is defined as shown in the following table:

Most Significant Byte

Least Significant Byte

15

14

13

12

11

10

9

8

7

6

5

4

3

2

1

0

Data Selection Code

Port Select

Bit assignments are included in the following table:

Bit

Field

Description

15...8

Data Selection Code (DS)

Indicates the diagnostic data to retrieve or to clear from the logical port. See the table below for valid values.

7...0

Port Select (PS)

Indicates the logical port number to retrieve the selected data from

  • 0x00 = the internal port of a device that supports an embedded switch or any single port not accessible externally

  • 0x01 to 0xFE = logical number of the desired port

  • 0xFF = the port the current request came in

This value should be 0xFF if the requested data is not port specific. See the Port Select Needed column in the table below for which Data Selection Code requires a valid port select value.

Data selection code

Data Selection Code

Diagnostic Data Retrieved

Port Select Needed

Type

0x00

Reserved

Public

0x01

Basic network diagnostics

Public

0x02

Ethernet port diagnostics

Yes

Public

0x03

Modbus TCP port 502 diagnostics

Public

0x04

Modbus TCP port 502 connection table

Public

0x05 to 0x7E

Reserved for other public codes

Public

0x7F

Data structure offsets

Public

0x80 to 0xFF

Reserved

Reserved

Response

Definition

Number of Bytes

Value

Server number

1 byte

0xFF

Function code

2 bytes

08 (0x08)

Sub-function code

2 bytes

22 (0x0016)

Operation code

2 bytes

1 ((0x0001) see the above list for operation code)

Diagnostic control

2 bytes

0x0100 (see the above list for diagnostic control)

Starting entry index

1 byte

0x00 (0 to 255)

Resetting Counters

The counters are reset to 0:

  • When they reach the maximum value 65535.

  • When they are reset by a Modbus command (function code 8, sub-function code 10).

  • When the power is cut off, or

  • When the communication parameters are modified.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.