DOCA0157EN-09

HeatTag Sensor Modbus Registers

The following table provides the registers that are available for HeatTag sensor.

Address

Register

No.

RW

XR

Unit

Type

Range

Invalid Value

Svd

Function Code

Description

0x0C3B

3132

2

RW

NA

°C

Float32

NA

0xFFC00000

N

03,

100-4

Internal temperature

0xC3E

3134

2

RW

NA

°C

Float32

NA

0xFFC00000

N

03,

100-4

Internal min temperature

0xC40

3136

2

RW

NA

°C

Float32

NA

0xFFC00000

N

03,

100-4

Internal max temperature

0x0CE1

3298

2

RW

NA

NA

UINT32

NA

0x00000000

N

03,

100-4

Validity of the alarm bitmap (register 3300)

  • 0 = Invalid

  • 1 = Valid

0x0CE3

3300

2

RW

NA

NA

UINT32

NA

0x00000000

N

03,

100-4

Alarms bitmap

0 = Alarm OFF

1 = Alarm ON 

Bit 8 = HeatAlarm status

Bit 10= Preventive maintenance on the device (fan error from HeatTag sensor)

Bit 11 = Device replacement (internal error from HeatTag sensor that implies to replacement)

0x0CF9

3322

1

RW

NA

NA

UINT16

0–190

0x0000

N

03,

100-4

HeatTag alarm type

0x0CFA

3323

1

RW

NA

NA

UINT16

0–3

0x0000

N

03,

100-4

HeatTag alarm level

  • 0 = No alarm

  • 1 = Low level alarm

  • 2 = Medium level alarm

  • 3 = High level alarm

0x0FA0

4001

2

RW

NA

°C

Float32

NA

0xFFC00000

N

03,

100-4

Temperature value

0x0FA2

4003

2

RW

NA

°C

Float32

NA

0xFFC00000

N

03,

100-4

Maximum value that the wireless device can read (maximum measurable temperature)

0x0FA4

4005

2

RW

NA

°C

Float32

NA

0xFFC00000

N

03,

100-4

Minimum value that the wireless device can read (minimum measurable temperature)

0x0FA6

4007

2

RW

NA

NA

Float32

NA

0xFFC00000

N

03,

100-4

Relative humidity value

Example: 50% represented as 0.50

0x0FA8

4009

2

RW

NA

NA

Float32

NA

0xFFC00000

N

03,

100-4

Maximum value that the wireless device can read (maximum measurable humidity)

0x0FAA

4011

2

RW

NA

NA

Float32

NA

0xFFC00000

N

03,

100-4

Minimum value that the wireless device can read (minimum measurable humidity)

0x0FAC

4013

2

RW

NA

NA

Float32

0–10

0xFFC00000

N

03,

100-4

Air quality index

  • 0 = Good without triggered alarm

  • 1–9 = Intermediate without triggered alarm

  • 10 = Bad with triggered alarm (register 3322 and 3323)

0x79C7

31176

1

RW

NA

NA

UINT16

0–2

0xFFFF

N

03,

100-4

Operation mode

  • 0 = Test mode (0–30 minutes after HeatTag sensor is powered on

  • 1 = Auto-learning mode (30 minutes–8 hours after HeatTag sensor is powered on)

  • 2 = Normal operation mode (>8 hours after HeatTag sensor is powered on)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.