DOCA0157EN-09

Environment Data

Ambient

Address

Register

No

RW

X

Unit

Type

Range

Invalid value

Svd

Function Code

Applicable Devices

Description

0x7530

30001

2

R

NA

°C

Float32

NA

0xFFC00000

N

 03,

100–4

H

Temperature of the 1st device

0x7532

30003

2

R

NA

°C

Float32

NA

0xFFC00000

N

 03,

100–4

H

Temperature of the 2nd device

...

...

...

...

...

...

...

...

...

...

...

...

...

0x75F6

30199

2

R

NA

°C

Float32

NA

0xFFC00000

N

 03,

100–4

H

Temperature of the 100th device

0x75F8

30201

2

R

NA

NA

Float32

NA

0xFFC00000

N

 03,

100–4

H

Relative humidity of the 1st device

0x75FA

30203

2

R

NA

NA

Float32

NA

0xFFC00000

N

 03,

100–4

H

Relative humidity of the 2nd device

...

...

...

...

...

...

...

...

...

...

...

...

...

0x76BE

30399

2

R

NA

NA

Float32

NA

0xFFC00000

N

 03,

100–4

H

Relative humidity of the 100th device

0x76C0

30401

2

R

NA

NA

Float32

NA

0xFFC00000

N

 03,

100–4

H

Air quality: Pre-alarm of the 1st device

0x76C2

30403

2

R

NA

NA

Float32

NA

0xFFC00000

N

 03,

100–4

H

Air quality: Pre-alarm of the 2nd device

...

...

...

...

...

...

...

...

...

...

...

...

...

0x7786

30599

2

R

NA

NA

Float32

NA

0xFFC00000

N

 03,

100–4

H

Air quality: Pre-alarm of the 100th device

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.