DOCA0157EN-09

Free Pairing of Wireless Devices with Webpages

All the wireless devices must be powered ON.

Step

Action

1

Launch the PowerTag Link webpage in the web browser.

2

Login to the webpage. Refer to Login into Webpages.

3

Navigate to Settings > Devices > Wireless Devices.

4

Click Start Scanning.

5

Stop scanning when all the devices are discovered, or click Start Scanning again to complete the scanning process.

Result: A list of paired devices is displayed.

6

Select the wireless device to configure and click Locate to find the device in the panel.

Result: The status LED of the selected device blinks fast green in the panel.

7

If one of the located wireless devices is not part of your selection, click Delete to reject the device.

8

Configure the wireless devices. Refer to Wireless Device Configuration with Webpages.

NOTE: The Modbus address assigned to the wireless devices can be changed after the pairing process is done.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.