DOCA0157EN-09

Unpairing Connected Wireless Devices

Step

Action

1

Navigate to Settings > Devices > Wireless Devices to view the list of the paired wireless devices.

2

Click the bin icon of the required wireless device to unpair.

Result: A message appears on the screen to confirm the removal of the wireless device from the configuration.

3

Click Yes to initiate the deletion process.

Result: Once the wireless device is successfully deleted, it will not be visible in the list of wireless devices discovered.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.