DOCA0157EN-09

About Alarms

Description

The Alarms page displays the active alarms. When an alarm is displayed, a notification is sent to the user by email (if the email service is enabled). An active alarm disappears when conditions of this alarm are not met anymore.

Step

Action

1

Launch the PowerTag Link webpage in the web browser.

2

Login with user name and password.

3

Click Monitoring > Alarms.

Parameter

Description

Alarm Type

Displays the type of an alarm when an alarm is occurred.

Alarm Value

Displays the threshold value of an alarm.

Asset Name

Displays the user-defined name of the alarm.

Usage

Displays the type of the usage.

Product

Displays the device type for which an alarm is configured.

Gateway

Displays the user-configured gateway of the device.

Email Content

Click Email to view the custom text of the email defined during an alarm configuration.

Date & Time

Displays the date and time of the configured alarm in yyyy/mm/dd hh:mm:sec format.

Click Change date & time to modify the date and time parameters in the Settings > General > Date and Time page.

Click Change alarm configuration to modify an existing alarm or to configure a new alarm in the Settings > Alarms > Alarm Configuration page.

Alarm Configuration Page

The Alarm Configuration page is used to configure alarms when there is an electrical event and communication loss.

Step

Action

1

Launch the PowerTag Link webpage in the web browser.

2

Login with user name and password.

3

Click Settings > Alarms > Alarm Configuration.

This page allows you to add a new alarm and edit the selected alarm from the list of events.

Follow the steps given in the table to add a new alarm:

Step

Action

1

Click Add Alarm to add a new event. You can create either generic alarm for the whole system or specific alarms to a selected device.

2

a

Select Generic Alarms for the Whole System, select when an alarm to occur, and then select the users to whom an alarm notification to be sent through email (optional).

b

Select Specific Alarms, select the required parameters, enter the threshold value that indicates for an alarm to occur, and then select the users to whom an alarm notification to be sent through email (optional). It is possible to add up to 25 specific alarms maximum.

3

Enter the Subject and Message of the email event (if necessary).

4

Click Apply Changes to save the settings. Click Cancel Changes to revert the settings.

NOTE: The email with custom text that uses characters such as à, è, ù, é, â, ê, î, ô, û , ë, ï, ü, ÿ, and ç are not shown correctly in the email but the generic text message is shown correctly.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.