DOCA0157EN-09

Wireless Devices Identification

Wireless Configured Devices – 100 Devices

Address

Register

No.

RW

X

Unit

Type

Range

Invalid Value

Svd

Function Code

Applicable Devices

Description

0x012C

301

1

R

NA

NA

UINT16

NA

0xFFFF

Y

 03,

100–4

A/M/R

IO/2DI

D/H

Virtual Modbus server address of 1st wireless node (1–245)

0x012D

302

1

R

NA

NA

UINT16

NA

0xFFFF

Y

 03,

100–4

A/M/R

IO/2DI

D/H

Virtual Modbus server address of 2nd wireless node (1–245)

...

...

...

...

...

...

...

...

...

...

...

...

...

0x018F

400

1

R

NA

NA

UINT16

NA

0xFFFF

Y

 03,

100–4

A/M/R

IO/2DI

D/H

Virtual Modbus server address of 100th wireless node (1–245)

0x0190

401

1

R

NA

NA

UINT16

NA

0xFFFF

Y

 03,

100–4

A/M/R

IO/2DI

D/H

Product ID of 1st device 

0x0191

402

1

R

NA

NA

UINT16

NA

0xFFFF

Y

 03,

100–4

A/M/R

IO/2DI

D/H

Product ID of 2nd device 

...

...

...

...

...

...

...

...

...

...

...

...

...

0x01F3

500

1

R

NA

NA

UINT16

NA

0xFFFF

Y

 03,

100–4

A/M/R

IO/2DI

D/H

Product ID of 100th device 

Wireless Device Metadata

Address

Register

No

RW

X

Unit

Type

Range

Invalid value

Svd

Function Code

Applicable Devices

Description

0x01F4

501

2

R

NA

NA

UINT32

NA

0xFFFFFFFF

Y

 03,

100–4

A/M/R

IO/2DI

D/H

Configuration counter.

Incremented each time a configuration data is modified on at least one of the virtual devices

0x01F6

503

10

R

NA

NA

ASCII

NA

0x00

Y

 03,

100–4

A/M/R

IO/2DI

D/H

Asset name (maximum 20 characters) given by the user to the 1st device. The name should be wriiten from MSB to LSB.

0x0200

513

10

R

NA

NA

ASCII

NA

0x00

Y

 03,

100–4

A/M/R

IO/2DI

D/H

Asset name (maximum 20 characters) given by the user to the 2nd device. The name should be wriiten from MSB to LSB.

...

...

...

...

...

...

...

...

...

...

...

...

...

0x05D4

1493

10

R

NA

NA

ASCII

NA

0x00

Y

 03,

100–4

A/M/R

IO/2DI

D/H

Asset name (maximum 20 characters) given by the user to the 100th device. The name should be wriiten from MSB to LSB.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.