DOCA0157EN-09

Reset Button

The Reset button is used to reset the PowerTag Link gateway.

There are two levels of reset:

  • Level 1: Press and hold the Reset button between 5 and 10 seconds until Status LED blinks in green. The parameters are retained and the mode of IP acquisition is set to DHCP mode. If you had set up a static IP address and lost your IP address, you can still retrieve your product using DHCP.

  • Level 2: Press and hold the Reset button for more than 10 seconds until Status LED blinks in red. The PowerTag Link gateway reboots and its parameters are reset to the factory settings.

    NOTICE
    HAZARD OF EQUIPMENT DAMAGE
    Do not switch off the gateway until the Status LED stops blinking in red for at least 30 seconds, as the reset level 2 is still in progress.
    Failure to follow these instructions can result in equipment damage.
    IMPORTANT: When performing a reset to factory settings on the PowerTag Link gateway, all wireless devices settings are cancelled and pairing of these devices in the gateway is also cancelled. Before performing reset to factory settings, it is recommended to do the following actions:
    1. Perform the backup action to avoid losing data.

    2. Unpair all wireless devices from the gateway.

    The consequences of reset level 2 are:

    • The user application name is set to myPowerTagLink-xxxx (where xxxx are the last four digits of mac address).

    • The building name becomes default.

    • The mode of IP acquisition is set to DHCP.

    • The password is set to the default value.

    • The panel information saved in the PowerTag Link gateway is erased.

    • The user accounts are erased (only default user accounts are retained).

    • The wireless device configurations are deleted.

    • The IP related settings are set to default value (date/time, DNS, IP filter, and email service). HTTPS is enabled.

    • Generic events are set to default configurations.

    • Specific alarm is deleted.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.