DOCA0157EN-09

Overview

The following sections describe the Modbus registers of the PowerTag Link gateway and the Modbus registers of the wireless devices connected to it. These registers provide information that can be read, such as electrical measures and monitoring information.

The Modbus registers are presented in the tables as per the type of device as follows:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.