DOCA0157EN-09

Alarm

Summary Registers: Alarm Data

Address

Register

No

RW

X

Unit

Type

Range

Invalid value

Svd

Function Code

Applicable Devices

Description

0x88B8

35001

2

R

NA

NA

UINT32

NA

0xFFFFFFFF

Y

 03,

100–4

Global alarm and event change counter.

Incremented when a new alarm or an event occurs on one of the devices.

0x88BA

35003

2

R

NA

NA

UINT32

NA

0x00000000

N

 03,

100–4

A/M/R/H

Validity of the alarm array of the 1st device (register 35004)

  • 0 = Invalid

  • 1 = Valid

0x88BC

35005

2

R

NA

NA

UINT32

NA

0x00000000

N

 03,

100–4

A/M/R/H

Alarm array bitmap of the 1st device

0 = Alarm OFF

1 = Alarm ON

Bit 0 = PowerTag energy – Voltage loss

Bit 1 = PowerTag energy – Overcurrent at voltage loss

Bit 2 = Reserved

Bit 3 = PowerTag energy – Overload 45%

Bit 4 = PowerTag energy – Loadcurrent loss

Bit 5 = PowerTag energy –Overvoltage 120%

Bit 6 = PowerTag energy –Undervoltage 80%

Bit 8 = HeatTag – HeatTag alarm

Bit 10 = HeatTag – Preventive maintenance on device

Bit 11 = HeatTag – Device replacement

0x88BE

35007

2

R

NA

NA

UINT32

NA

0x00000000

N

 03,

100–4

A/M/R/H

Validity of the alarm array of the 2nd device (register 35008)

  • 0 = Invalid

  • 1 = Valid

0x88C0

35009

2

R

NA

NA

UINT32

NA

0x00000000

N

 03,

100–4

A/M/R/H

Alarm array bitmap of the 2nd device

0 = Alarm OFF

1 = Alarm ON

Bit 0 = PowerTag energy – Voltage loss

Bit 1 = PowerTag energy – Overcurrent at voltage loss

Bit 2 = Reserved

Bit 3 = PowerTag energy – Overload 45%

Bit 4 = PowerTag energy – Loadcurrent loss

Bit 5 = PowerTag energy –Overvoltage 120%

Bit 6 = PowerTag energy –Undervoltage 80%

Bit 8 = HeatTag – HeatTag alarm

Bit 10 = HeatTag – Preventive maintenance on device

Bit 11 = HeatTag – Device replacement

...

...

...

...

...

...

...

...

...

...

...

...

...

0x8A46

35399

2

R

NA

NA

UINT32

NA

0x00000000

N

 03,

100–4

A/M/R/H

Validity of the alarm array of the 100th device (register 35400)

  • 0 = Invalid

  • 1 = Valid

0x8A48

35401

2

R

NA

NA

UINT32

NA

0x00000000

N

 03,

100–4

A/M/R/H

Alarm array bitmap of the 100th device

0 = Alarm OFF

1 = Alarm ON

Bit 0 = PowerTag energy – Voltage loss

Bit 1 = PowerTag energy – Overcurrent at voltage loss

Bit 2 = Reserved

Bit 3 = PowerTag energy – Overload 45%

Bit 4 = PowerTag energy – Loadcurrent loss

Bit 5 = PowerTag energy –Overvoltage 120%

Bit 6 = PowerTag energy –Undervoltage 80%

Bit 8 = HeatTag – HeatAlarm

Bit 10 = HeatTag – Preventive maintenance on device

Bit 11 = HeatTag – Device replacement

0x8B12

35603

1

R

NA

NA

UINT16

NA

0x0000

N

 03,

100–4

H

HeatTag alarm type of the 1st device – Value between 1 and 190

0x8B13

35604

1

R

NA

NA

UINT16

NA

0x0000

N

 03,

100–4

H

HeatTag alarm type of the 2nd device – Value between 1 and 190

...

...

...

...

...

...

...

...

...

...

...

...

...

0x8B75

35702

1

R

NA

NA

UINT16

NA

0x0000

N

 03,

100–4

H

HeatTag alarm type of the 100th device – Value between 1 and 190

0x8B76

35703

1

R

NA

NA

UINT16

NA

0x0000

N

 03,

100–4

H

HeatTag alarm level of the 1st device

  • 0 = Good

  • 1 = Low

  • 2 = Medium

  • 3 = Bad

0x8B77

35704

1

R

NA

NA

UINT16

NA

0x0000

N

 03,

100–4

H

HeatTag alarm level of the 2nd device

  • 0 = Good

  • 1 = Low

  • 2 = Medium

  • 3 = Bad

...

...

...

...

...

...

...

...

...

...

...

...

...

0x8BD9

35802

1

R

NA

NA

UINT16

NA

0x0000

N

 03,

100–4

H

HeatTag alarm level of the 100th device 

  • 0 = Good

  • 1 = Low

  • 2 = Medium

  • 3 = Bad

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.