DOCA0157EN-09

Characteristics

Circuit Breaker Rating

Address

Register

No.

RW

X

Unit

Type

Range

Invalid Value

Svd

Function Code

Applicable Devices

Description

0x1388

5001

1

R

NA

A

UINT16

NA

0xFFFF

Y

 03,

100–4

2DI

Circuit breaker rating of the 1st device

0x1389

5002

1

R

NA

A

UINT16

NA

0xFFFF

Y

 03,

100–4

2DI

Circuit breaker rating of the 2nd device

...

...

...

...

...

...

...

...

...

...

...

...

...

0x13EB

5100

1

R

NA

A

UINT16

NA

0xFFFF

Y

 03,

100–4

2DI

Circuit breaker rating of the 100th device

Power Factor Sign

Address

Register

No.

RW

X

Unit

Type

Range

Invalid Value

Svd

Function Code

Applicable Devices

Description

0x13EC

5101

1

R

NA

NA

UINT16

NA

0xFFFF

Y

 03,

100–4

R

Power factor sign convention of the 1st device

0x13ED

5102

1

R

NA

NA

UINT16

NA

0xFFFF

Y

 03,

100–4

R

Power factor sign convention of the 2nd device

...

...

...

...

...

...

...

...

...

...

...

...

...

0x144F

5200

1

R

NA

NA

UINT16

NA

0xFFFF

Y

 03,

100–4

R

Power factor sign convention of the 100th device

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.